Hi
what is the current consumption of this chip in AVDD@3.3v and vddio @1.8 v rails it is not clear in the datasheet .has any one used this chip do u have any details regarding this ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
what is the current consumption of this chip in AVDD@3.3v and vddio @1.8 v rails it is not clear in the datasheet .has any one used this chip do u have any details regarding this ?
Hi Luis Fernando Rodríguez S
Thanks for the reply, In the datasheet iovdd is used as 3.3 V
In the processor i am using the i2s interface all are of 1.8v logic
so i have connected iovdd as 1.8v in the tlv320dac3120 chip ,in the data sheet of tlv320dac3120 the typical value of iovdd is 3.3 shall I use iovdd as 1.8v ?
The analog input I am not using in my design do i have to terminate it or can be left floating? (not using record and playback ) in this case Do i have to provide AVDD input ?I am not using HP pin as well can I leave this floating?