The setup I have is a TUSB2046 hub, connected to qty 3 PCM2706 & qty 1 PCM2900E. I went based off page 15 of the TUSB data sheet schematic: http://www.ti.com/lit/gpn/tusb2046b
I am using the TPS2044, and have the OC pins & EN pins directly connected to the hub, as shown in the schematic. BUT, if you look at the schematics listed on pages 15, 19 & 20, on the TPS2044 data sheet, it shows a resistor & a 3.3V supply going to the OC pins: www.ti.com/.../getliterature.tsp
1) Should I run 3.3V to the OC Pins?
2) And if so, what resistor value do I put there???
The reason I ask, is because my sound cards are not recognized in Windows. Here's some details:
-Windows recognizes the hub, as a generic hub. So I get the impression that the hub is operating properly.
-The OC pins on the hub/TPS2044 are active low, and the PWRON pins are high. Which I interpret it to be saying that the protection mode has been set and the sound cards have been disabled.
-Both the 2900 & 2706 SSPND pins are low.
-I am running in Bus Powered mode, since I need the 2706 to be able to do custom names, and the only way it can do custom names is if it is bus powered.
-I have the 2706 HOST set to low, so that it is running at 100mA.
-The voltage going to the 2900 pin 3 is 5V, which is good.
-The voltage going to the 2706 pin 24 is only 2.8V.
Thank you for your help! And please let me know if you have any questions. THANKS!!!!