Hi there, I'm trying to get an idea of how much the TLV320AIC3110 Stereo Audio Codec will draw when both of it's 1W speakers are active. The "TLV320AIC31xx and TLV320DAC31xx Power Consumption"Characterization" App note Pg. 9 has a bunch of power consumption data using various processing blocks, but they all sit at around 75mA. The datasheet specifies a maximum output power of 540mA, so not sure where this 75mA power consumption figure fits in, when both Class-D driven speakers are going. Could you shed some light on this? I would expect the max power consumption to be 540mA x 2 (2 speakers - 100% efficiency!), plus whatever the Analog/Digital circuitry in the chip are drawing.
Many Thanks,
Dave