Hi,
Does SRC4392 only perform the internal audio processing with the audio data word lengths up to 20 bits if the following channel status bit is included in the audio data which is input via the S/PDIF input port ?
Or, does SRC4392 perform the internal audio processing with the audio data word lengths up to 24 bits regardless the channel status bit ?
<Channel Status Bit>
status bit32 : 0 (Word Length : 20 bits)
status bit35 ~ bit33 : 000
Best regards,
Kato