Can you tell me why I'm consistently seeing a stereo 20 kHz sine wave with no phase shift between L/R with 48 kHz or 96 kHz, but the same signal has ~ -37.41° shift with 192 kHz.
Also, testing at various frequencies show the following results, (all at 192kHz sampling)...
@ 1kHz, I see about a -1.5° phase shift; @ 5kHz a -9.36° shift; 10kHz a -28.08° shift
Best Regards,
Jim