Other Parts Discussed in Thread: PCM5100
Hello,
I am interfacing PCM1861 and PCM5100 to ADAU1701 audio processor. The audio processor is using a 12.288MHz crystal and the sampling rate is set to 48KHz
The ADAU1701 is I2S clock master and both the ADC and the DAC are slaves and share the BCLK and LRCLK lines.
I have no issues with the PCM5100 and it is working correctly.
However, there is no sound from the ADC.
I have attached the schematics of the ADC and the DAC sections.
Do let me know if you need any further information from my side.
Thanks!!PCM1861 issue.doc
Ravindra.