Good morning
I have started to prove the src4392EVM-PDK with simples instructions. Then I try to read what I have written. However I see that bits are all zeros. Why this is happened?
Thanks and Regards
Alberto de la Peña
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good morning
I have started to prove the src4392EVM-PDK with simples instructions. Then I try to read what I have written. However I see that bits are all zeros. Why this is happened?
Thanks and Regards
Alberto de la Peña
Hi, Alberto,
This behavior seems odd, have you tried reading a different register?. There should be no issue with the read/write process.
I have ordered an EVM so I can replicate this issue, but it is still a couple days away from arriving. Please try the same process with different registers.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Good Morning
I have proved writting and readind in other registers and there is no problem. Only with the register 01 in page 0 occurs that issue.
There is other trouble, when I read one register, the value is correct, but if i read several registers in one instruction the value is
replicated in the other registers. If I read the registers one by one, the values are rigth. I attach one capture to clarify this question.
Regards
Alberto de la Peña