I am using the PCM1794A in a application where it receives the I2S signal from an S/PDIF receiver chip (Cirrus CS8416).
The CS8416 has an output which indicates loss of signal on the S/PDIF side, I am using this signal to mute mute the PCM1794A on pin 10.
The issue that I am having is that while the PCM1794A is muted in this way there is noise on the output which sounds like hissing.