Tool/software: Linux
Hi, I'm new to codec and got a problem.
I am using Beaglebone black,tlv320aic3104 on custom cape.
I used MCLK, BCLK, WCLK, DIN pin to make sound .
( I am using sdk, am335x-evm-03.03.00.05)
I enabled oscillator on beaglebone black(I used GPIO1_27 to enable it) to make 24.576 MHz clock to MCLK.
I used device tree file to configure hardware.
To test it, I used speaker-test command.
and I could see MCLK(3), BLCK(4), WCLK(2), DIN(1) output. see below picture.
But, I could not hear anything from speaker attached to HPLOUT/HPROUT.
so below is HPLOUT/HPROUT.
Only thing I could see is little increase in voltage (when I used 'speaker-test' command)
I'm waiting for advise.
Thanks.