DEARS.
The PCM4201 input type is difference.
Can I PCM4201 analog input type be used as Single-End?
What is the SE input type product with a similar specification of pcm4201?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DEARS.
The PCM4201 input type is difference.
Can I PCM4201 analog input type be used as Single-End?
What is the SE input type product with a similar specification of pcm4201?
Thank you.
Hi, Henry,
The PCM4201 supports only differential inputs. For the operation of the device with a single-ended audio source, an input buffer is recommended to convert to Differential signal from the SE source.
A SE-Diff buffer circuit is provided in page 17 of the datasheet.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer