Hello
I want to use a PCM5310 (Audio Codec) combined with a TAS6424-Q1 (Class-D Audio Amplifier). There is no I2S device connected to the PCM5310 who can provide the clock for the internal DAC and ADC.
Can I connect an oscillator to the pin 51 (SCK6, PORT-6 system clock) and leave the other pins of channel 6 open to distribute the clock internally to the ADCs, DACs and outputs (Port1 and 2) as shown in the attached block schematic?
Kind regards,
Christian Ruder