This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3101EVM-K: TLV320AIC3101 NOISE SO MUCH

Part Number: TLV320AIC3101EVM-K

TODAY I encouter a problem。my  schematic is as follows。now the value of C20 and C24 is 0.1uf. and the resistor  R218 and R216 is not populated.my platform is MCIMX6Q5EYM10AD。 I have two single  end input  AUDIO2_IN and AUDIO1_IN ,which connected to  outer interface ,when i test  i  connect a line jack to  AUDIO2_IN and AUDIO1_IN and gnd, and  connected another jack to LINEOUT_L and  LINEOUT_R  and gnd.then the program  make a loop between audio2_in  and  lineout , i  play a music into  the audio_1in and  audio2_in,while i hear  the music through a Jack  connected to  lineout。I  find there SO MUCH noise  ,what was wrong ,can somebody  help me ?very worried