Hello.
I have a question about TLV320AIC3254 mixer function. Can I mixer Digital Mic(Pin 8 and Pin 11) and LINE-IN(IN2 Pin 15 and Pin16) to I2S out.
If Yes. Please kindly provide the Register for our reference. Thanks for Help.~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
I have a question about TLV320AIC3254 mixer function. Can I mixer Digital Mic(Pin 8 and Pin 11) and LINE-IN(IN2 Pin 15 and Pin16) to I2S out.
If Yes. Please kindly provide the Register for our reference. Thanks for Help.~
Hi, AJ,
Unfortunately, the mix between digital mic and line inputs is not possible with this device. This is because when using digital microphone, the ADC connection to the internal filters is replaced with the digital mic interface. Only individual operation is supported.
The only possible way to mix digital mic signal with analog in signal would be to use one channel for the analog input and one channel for the digital mic, then mix these with the miniDSP of the 'AIC3254.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer