Other Parts Discussed in Thread: TLV320AIC3262
Hi Team,
Do we have any audio data converters that can take two separate I2S inputs and output a single mixed mono result? I noticed the AIC3204 has a primary and secondary I2S inputs but it looks like the pin muxing doesn't allow this. Are there some data converters that can do this? It's okay if this is mixed in the analog or the digital domain, as long as it outputs on the same single speaker.
I'm trying to find a replacement to the MAX98089 which has two I2S inputs and can do this. the LM49350 also looks like it has two inputs, but I'm not sure if it would work and I'd prefer to use a part with an EVM.
Thanks!
Nate