Other Parts Discussed in Thread: WL1833
Tool/software: Linux
Hi All,
I am using TLV320AIC3106Q and WL1833Q to form a PCM/I2S (GPIO1/GPIO2/MFP3/DOUT) connection for Bluetooth HFP application.
I am trying to used the following FD06 command to setup WL1833Q Bluetooth to Master role, and the TLV320AIC3106Q codec would be Slave role. The thing is after I put this command modification into my TIInit_11.8.32.bts, and bring up the system (i.MX6Q), I can not detect the BCLK from my oscilloscope. There is no BLCK from this I2S/PCM. Is my command wrong or is it needed a special configuration?
Command:
Send_HCI_VS_Write_CODEC_Config 0xFD06, 0x0200, 0x00, 0x00003e80, 0x0001, 1, 0x01, 0x00, 0x0010, 0x0001, 1, 0x0010, 0x0001, 0, 0x00, 0x0010, 0x0011, 1, 0x0010, 0x0011, 0, 0x00
I am appreciated any comment or suggestion.
Thanks.
-Justin