Hello,
Currently I use the below circuit for receiving audio inputs to PCM1861
There is also a voltage scaler before the above circuit.
Can you please guide me for improvements to the input circuitry?
thanks
rifo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Currently I use the below circuit for receiving audio inputs to PCM1861
There is also a voltage scaler before the above circuit.
Can you please guide me for improvements to the input circuitry?
thanks
rifo
Hi, Rifo,
The PCM1861 is a flexible device which input stage can support several configurations as long as the voltage on the input pins is under the specifications from the datasheet. The circuit you are currently using seems fine, I don't think a lot of improvement is necessary for general applications.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer