Our company makes equipment to find victims in the rubbles.
I would like to update the electronics in the devices.
The device works as an intercom. At one end of the headset and on the other loudspeakers with a microphone.
I need to:
1) Get very high microphone sensitivity with good AGC.
2) get sound without interference.
3) Suppress the echo from the speakers.