If the PCM2906 chip is setup like the schematic in the data sheet i.e. the HID bits are pulled up by the suspend pin, will the device generate an interrupt for the HID bits when it comes out of suspend?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the PCM2906 chip is setup like the schematic in the data sheet i.e. the HID bits are pulled up by the suspend pin, will the device generate an interrupt for the HID bits when it comes out of suspend?
Hi, Matt,
The part should get the state of HID once suspend state is finished. However, if this is done, you might see strange behavior on the volume of the device as the interface will try to adjust the volume up/down/mute at the same time.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer