Hello All,
We are testing TLV320AIC3104 IC using Automatic test equipment (Advantest V93K). By making AIC3104 as slave, we could write all the registers and read back the same except Regiter-86 and Register-93. These two registers are responsible for LEFT/RIGHT_LOP/M Output Level Control Registers.
In these registers, the D1(read only) bit is expected to be '0' - which means " all programmed gains are applied". But we are reading '1' . Since it's a read only bit, is any other register need to be programmed additionally.
iovdd 3.3 V
dvdd 1.8 V
avdd 3.3 V
drvdd 3.3 V
Tried with both 10K and 1K pull up on SCL, SDA.
Please help us. Are we missing something in programming.