Why three MIC inputs are given in the TLV320AIC3120 ? from the block diagram one of the MIC is connected to negative input of Comparator used to fed PGA input.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Why three MIC inputs are given in the TLV320AIC3120 ? from the block diagram one of the MIC is connected to negative input of Comparator used to fed PGA input.
AMIT,
I don't see this comparator you're talking about. there are there are selectable gain/input impedance blocks, mixers, and the PGA.
The inputs are flexible.
1. Mic1LP and Mic1LM can be used as a single Differential input by connecting MIC1LM to the negative input of the PGA.
2. all three inputs can be used simultaneously as Single ended inputs. in this case VCOM should be connected to the negative terminal of the PGA.
3. MIC1LP, Mic 1RP can bypass the ADC and be mixed with the output, while Mic 1LM can be used as a single ended input.
obviously there are variations on these, but these are the 3 main ways we see the 3 inputs used.
best regards,
-Steve Wilson
thanks.
I have used MIC1Rp as input and MIC1LP and MIC1RM is not used.VCOM is programmed for negative input of PGA.
is it OK? I programmed Codec register for the selection i used.
Dear Steve
I am using two microphone, one of mic is permanently connected to MIC1RP input and MIC1LP input is used for jack based Headphone MIC. when i am reading register 0x2E on page 0 to headphone insertion removal detection. This gives me wrong indication.