Hello all!
My customer uses audio codec TLV320AIC3109-Q1 + GSM modem EHS5 (datasheet is here).
The modem uses DAI/PCM digital audio interface.
Recently the customer had a problem with clocking of the codec (see e2e thread here) which was successfully solved.
Now the customer is working with microphone and facing with the following problem: sound from the mic which comes to EHS5 through the codec is dirty or absent. It is depend on MICBIAS voltage:
2.5V reference → sound is very noisy
2.0V reference → there is no sound at all
We suppose that the reason can be in MICBIAS configuration register. Below you can find codec configuration which used by the customer. Could you please have a lokk and advice what can be wrong.
300000
300180
3002AA
300381
3004C0
300500
300600
300708
300800
3009C0
300C80
300E80
300F76
301000
301384
301940
301A80
301BFE
301C00
302440
302506
302600
302900
302B00
303D80
304109
304809
305E82
306500
306600
Thanks in advance