Hi ,
I am t using TLV320AIC3120,
but I am getting faint click sound which is hardly audible, but I need longer beep sound.
I need this EVM for BEEP generation only, I am not using I2S, just configuring Registers with I2C,
Configuration which i have done is written below
can you help me out on this,
#Select Page 0 w 30 00 00 # PLL_CLKIN = MCLK, CODEC_CLKIN = MCLK ######## MCLK=1 MHz w 30 04 03 & #0x07
# r=1,p=1;
w 30 05 92
# j=32
w 06 10
# D=0
w 07 00
w 08 00
# DAC Instruction set PRB_P25 w 30 3C 19 # NDAC ON div=1 w 30 0B 82 # MDAC ON div=2 w 30 0C 84 # DOSR = 144 w 30 0D 00 w 30 0E 90 # DAC Volume -0 dB w 30 41 30 # DAC mute off w 30 40 04 # DAC power up w 30 3F 80 w 30 24 00 w 30 25 90
# Select Page 1 w 30 00 01 # Class d driver power up w 30 20 86
#DAC routed to mixer amp
w 30 23 40 # Class D route enable w 30 26 00 # Class D output driver mute off w 30 2A 1C ####Fs=50 Khz, Fin=1kHz. # Select Page 0 w 30 00 00 # Beep length=004E20 w 30 49 00 w 30 4A 4E w 30 4B 20 # sin wave coeffi=1008 w 30 4C 10 w 30 4D 08 # cos wave coeffi=7EFD w 30 4E 7E w 30 4F FD # Beep generate 0 db w 30 47 80
Thanks,
Zanza