• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » Audio Converters » All Tags » dac
Share
Audio Converters
  • Forum
  • E2E Wiki

Browse by Tags

Audio Converters

Welcome to the Audio Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
dac
  • ADC
  • AIC_codec
  • aic23
  • AIC3104
  • aic3106
  • AIC310X
  • AIC3204
  • AIC3254
  • AIC3254 filters decimation interpolation adc dac
  • AIC3254 PurePath
  • Audio
  • audio codec
  • audio codecs
  • codec
  • Driver
  • I2C
  • I2S
  • noise
  • TLV320ADC3101
  • TLV320AIC23B
  • TLV320AIC3104
  • TLV320aic3204
  • TLV320AIC3254
  • TLV320AIC3254 EVM
  • TLV320DAC3100
Related Posts
  • Forum Post: PCM1704 specifications

    Kurt G Kurt G
    I'm really hoping somebody can help me. I need to know the input impedance/capacitance for the inputs of the PCM1704U, particularly BCLK, WCLK and DATA. An IBIS model for this chip would also be extremely helpful. I have checked the datasheet as well as every other resource related to this chip...
    on Jan 13, 2010
  • Forum Post: PCM1704 BCLK pin impedance

    Kurt G Kurt G
    What's the input impedance of this pin? This info is needed for line termination. Thank you.
    on Jan 23, 2010
  • Forum Post: PCM1794A imprecise reset documentation

    Pavel Ruzicka Pavel Ruzicka
    I had troubles with PCM1794A, that it doesn't reset after power-up. In datasheet is info, that PCM1794A has internal reset circuit and possibility to use external reset. There are not information, that when I want use only internal reset, I must have externally pulled-up reset pin to VDD or VCC....
    on Feb 3, 2010
  • Forum Post: PCM1704 seperate power supplies

    Kurt G Kurt G
    Hello. I need to power this chip from seperate analog/digital supplies. That is, +Vdd,-Vdd,+Vcc,-Vcc will be 4 seperate power supplies. What is the maximum allowable difference in voltage between the digital and analog side? That is, for example, the difference between +Vdd and +Vcc? The datasheet...
    on Feb 16, 2010
  • Forum Post: TLV320AIC23B output problem

    Javier Gr Javier Gr
    Hello, I'm working with the stereo codec TLV320AIC23B and I can´t manage to get an audio signal at the output. What I get is a DC level. I have configured the device in DAC mode using I2C. It's working as slave. The MCLK frequency is 12.288 MHz, the BCLK frequency is 1.536 MHz and...
    on Mar 23, 2010
  • Forum Post: Re: TLV320AIC23B output problem

    Javier Gr Javier Gr
    Hello Vikas, I disabled these bits because according to the application note 'Dynamic Behavior of the TLV320DAC23 and the TLV320AIC23B' if OSC is disabled, MCLK still functions. And regarding to the CLK bit, it powers off the CLKOUT pin because we don't need it. Anyway, I also tried...
    on Mar 23, 2010
  • Forum Post: Re: TLV320AIC23B output problem

    Javier Gr Javier Gr
    Hello Vikas, We have placed the TLV320AIC23B in our own audio board. I have attached the schematic of the circuit, where capacitors S12 y S13 are not mounted for testing. I have one question related to the frequency of BCLK. At the end of page 24 of the datasheet it is said that when the codec...
    on Mar 24, 2010
  • Forum Post: PCM1792(A) - Various Questions

    Jens Bauer Jens Bauer
    Hi, I'm a 'newbie' in this area; currently developing hardware for (and software to control) a PCM1792A. A few questions arose in my mind. 1: Why is the DSD schematic different from the PCM schematic ? - isn't DSD just an input format? 2: What's the max. available sampling...
    on Jul 23, 2010
  • Forum Post: Re: 32bit version of the PCM1792A or DSD1792A

    Jens Bauer Jens Bauer
    I agree as well. The S/N virtually eats up the extra 8 bits, but if using two DACs in monoaural mode, one could get a little closer. My guess is that the cool dudes behind the DACs are most likely working on something awesome right now. If not, I'd suggest that they make an 'easy enhancement'...
    on Jul 26, 2010
  • Forum Post: Re: Sampling rate of TLV320AIC3204.

    Fangyi Chen Fangyi Chen
    Hi, J Thanks for the reply. I have further questions in using the audio codec to generate a high frequency tone. 1. Sampling points. Despite the Nyquist, a sine wave may have to have more than 10 sampling point to show its shape. A codec dac is usually limited by its relatively low sampling rate...
    on Sep 23, 2010
  • Forum Post: Re: Sampling rate of TLV320AIC3204.

    Fangyi Chen Fangyi Chen
    Thanks again, J. You seemed to say that as long as the sine wave frequency is lower than 1/2 (Nyquist) sampling rate, there should be no problem. But I would like to confirm this with you again. The reason that I am skeptical about this is my experience with a MATLAB demo. It is in the data acquisition...
    on Sep 24, 2010
  • Forum Post: Difference between PCM1796 and PCM1792A

    Daniel XXX Daniel XXX
    Hello, My name is daniel and I am new to this forum. I am interested in Hifi and I have some questions regarding to Audio Converters of Texas Instrument. I own a Soundcard with an PCM1792A Chip. The sound is quite good but like all Hifi freaks i always try to increase my sound quality. So i was looking...
    on Oct 2, 2010
  • Forum Post: AIC3254 problems with right and left DACs

    Gonzalo R. Gonzalo R.
    Hi, I'm having trouble with output channels in AIC3254. This is my process, the simplest process, uniquely for testing output channels: I've modified registers and left channel is routed via HP (LDAC_P -->HPL, LDAC_N-->HPR), and right channel is routed via LO (RDAC_N-->LOL...
    on Dec 29, 2010
  • Forum Post: PCM1774 and IIS input

    Martin Sauer Martin Sauer
    Hello, I want to use the PCM1774 in our design for analog and digital audio muxing. I get the digital audio data from CS8416 (digital audio interface receiver) in I2S format. I set the configuration registers descripted in the datasheet but don't get an audio signal at the ouput if I have a...
    on Feb 16, 2011
  • Forum Post: DSD1791A: Dynamically varying the sampling freq to change the freq of the output...

    Matt Hosler Matt Hosler
    I am interested in using the DSD1792A DAC for an unconventional application. We need to produce a 20-40 kHz sine wave with 120 dB of dynamic range as a feedback signal to a sensor. We want to output the same values of a sine wave (min,max,and zero), but dynamically vary the sampling frequency to change...
    on Mar 7, 2011
  • Forum Post: DSD1608 Support the McBSP?

    Cristian Sicilia Cristian Sicilia
    Hi, I'm new on audio device, and tryng to add to a beagleboard tree audio output. Beagleboard have a McBSP on expansion port, but in the DSD1608 I see more than one data in (seems a McASP), can I connect a DSD1608 to with a McBSP? Or if exists a multiple (better) or a single (that I can...
    on Jul 19, 2011
  • Forum Post: Re: DSD1608 Support the McBSP?

    Cristian Sicilia Cristian Sicilia
    Hi, would be perfect! But I not understood how to connect more than one DAC in cascade. In some example McBSP: - FRX is connected to FS - CLKX to SCLK - DX to DIN - DR to DOUT now all same connection for second device, except for FS, that is connected to FSD of first DAC device....
    on Jul 20, 2011
  • Forum Post: Multi Channel Audio DAC

    Viral Sachde Viral Sachde
    Hi, I am designing device having one multi-channel (6 Channel) audio output. For Audio DAC, I am considering DSD1608 or equivalent Multi channel Audio DAC. As per my understanding, I will need 3 IIS port. Can someone suggest me any processor having 3 or more IIS or audio port. Also, is it possible to...
    on Aug 6, 2011
  • Forum Post: Re: PCM1609 - Communication with MCU

    Radim Voříšek Radim Voříšek
    Hi Patrick, does PCM1609A need for the Communication with MCU a SCKI Signal? or this Signal is used only for Filter, DAC ...??? is there any 1:1 Replacement? thank you for your answer. with Regards, Radim.
    on Sep 16, 2011
  • Forum Post: PCM1792a and OPA1632 together

    Alexei Petrov Alexei Petrov
    Hello. I have some questions on application PCM1792a. 1. How much precisely it is necessary to withstand ground potential on the current outputs of a DAC PCM1792a (Iout pins)? If the potential changes in small limits - for example, from-0.1 volt to +0.6 volt, whether to degradation DAC parameters (TDH...
    on Sep 16, 2011
  • Forum Post: PCM4104 THD+N performance issue

    milk wang milk wang
    In our DS, we show that we can have -100dB ~ -94dB in Fs:48kHz, Fin:1KHz, 0dBFS. But while our customer uses it, it can only perform -8xB in each channel (based on the schematic of our EVM) and the parameter could not be acceptable. They also use our EVM to do the test but it has the same performance...
    on Feb 9, 2012
  • Forum Post: Re: TLV320AIC3110 codec linux driver

    Pradeep TR Pradeep TR
    We have used Audio Codec TLV320AIC3110 in our custom boad with TI8148 in EVM we have TLV320AIC3106 which is not register level compatible with the 3110. So we are able to configure Audio Codec it is connected to McASP2 as much as same in the EVM with pin to pin compatible in our custom board...
    on Feb 18, 2012
  • Forum Post: DAC Dynamic Range, SNR

    Behnam molaee Behnam molaee
    Hi My question is related to the dynamic range (DR) of the DAC of an audio codec such as PCM3060 . In PCM3060 (for instance) the DR of the DAC is 112dB. There is also an internal volume control between 0 to -100dB. If I've understood well, the dynamic range is given when the volume is set...
    on Mar 13, 2012
  • Forum Post: Re: PCM1774

    Carmelo Garcia Carmelo Garcia
    Hello Don. I am in the same situation as Slomi. I have the PCM1774 connected to i2c in my AM1808 custom board. This board is working on linux, and I would like to know how to get the PCM1774 working through i2s. Do I need to init the device in the linux kernel, or will i2s (alsa) find...
    on Mar 27, 2012
  • Forum Post: TLV320AIC3254 Producing Unwanted Spectra

    3441533 3441533
    Hi, We have configured the CODEC and are passing the I2S data corresponding to a 1KHz sinewave. Sampling rate is 96KHz. We are using both internal LDOs so only a +3V3 power rail is used. We are measuring at the CODEC output pin (LOL) with nothing else on that net. When the output is connected to...
    on Apr 18, 2012
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use