Welcome to the Audio Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: AIC3104 ADC HPF coefficient
How do you program the AIC3104 1st order HP filter?
A: Re: AIC3104 ADC HPF coefficient
There are 3 steps to load programmable coefficients for ADC First-Order HPF: ( need to be in order)
1. Load coefficients N0, N1, D1 to Page 1 / Register 65 - 70 and Page 1 / Register 71 - 76
2. Select the programmable coefficients (Go to Page 0 / Reg 107, and Set D7 = 1 and D6 = 1)
3. Enable ADC high-pass filter ( Go to Page 0 / Register 12, you can set D7-D6 to 01, or 10, or 11). Please ignore the -3dB frequency selection in this register, because in the programmable case, the real -3dB frequency is determined by the coefficients.