Q: Max Gain error AIC3101

The DAC gain error for the AIC3101 is listed at -0.2 dB typical but there is no max number.  Is this information on the max available or does TI have any guidance on what should be expected?

A: Re: Max Gain error AIC3101

Original bench characterization showed as much -.6 dB to - 3 sigma on the left line outputs. However we don't measure this in production so we can't give a max or a min. The original bench test was on a fairly small sample size so we are not sure how much you can draw from that. The number would change if you were looking at the HP outputs.