Dear TI Experts,
I need some help to understand some parameters / values of the ADS1258
Using the ADCpro sw, here is the result:
Q1.: As you can see the VCC and Vref values are about 2.5V. Could you tell me why? I suppose this value should be around 5V? I am using Unipolar power source (included in the package 6V power supply)
S2 switches are in Center position for DAC ref. voltage. But When I set the switches to the left the result is the same.
The ADS1258EVM manual Page 8 - 5 Voltage Reference section says: The output of the dac is multiplied by to giving a range approx. 0-5V.
Q2.: Does it mean, the maximum value of DAC on the front panel is 2.5?
My second problem is related to VREF and the calculation of the measured value results from the ADC.
VREF: According to the ADS1258 datasheet, Vref = Vrefp - Vrefn. On the page 25. equation says: 1LSB = Vref / 780000h. - This is the way how I can calculate the Voltage from the ADC
Q3.: Is Vref in this equation equals to the REF value that I can get back from the Channel Data format when CHID[4:0] = 1Dh ? So If i want to get an accurate Voltage result, first I am going to divide the REF value (External Reference) by 7800000h and then multiply this value by the Channel Data value ( after the conversion from Binary2's).
Looking forward your kind reply.