Hi,
I have a board with a daisy chained ADS131E04 master, first ADC, and ADS131E08 as slave, 2-the ADC. When i power up the board (cold reset), the 2-the ADC never initializes OK to 4Kbps sampling mode. I need an extra warm master reset to the whole board and then the 2-the ADC configures OK. I checked the POR sequence described in the ADS131 datasheet and also the sequence of 5V and 3V3 en all is following the specs.
All ideas welcome...
Regards,
Koenraad