Hello support/comunity
I make a board with the example electrical schema 8.2.1 (Analog output Module for PLC-and DCS Based Industrial -Control Systems) page 38 the only difference between this one an the one that I make is a pull down resistor on pin 7 on the ISO7631 that control the enable of SDO communication pin because we have another device on this bus, so here is dude my partner Nicolas is working with the code and make the following code cited below.
The code write 0x00FF, and the DAC answer with high level for an short period on the SDO pin without any clock and then return 0x00F0, the current output still in 0.
Could you please help us to find what is wrong here, in this code or show us an example if you have it?
Thanks in advance
PHY_INA = 0; // TO CLEAR
//For write the DAC