Hello!
As seen before in forum, I have the issue with the EVM:
After starting up the ADS1x98/8REKG-FE EVM Evaluation Software I got the following sequence:
- Reading Binary file
- Downloading binary file
- USB connection established
- Download successful
- DSP not ready...retrying
- Popup "The firmware load has failed due to connection timeout..."
- Popup "Connection and FW Load Failed! Please check your connection/configuration and try again"
and Retry button does not help.
USB device is exists in Device Manager, and external power +/-10V applyed to +/-VA, and -5V applyed to -5VA at J14.