hi,
I recently have a problem about single-shot mode of ADS1115Q1 for ADC, when supply power +5V for ADS1115, and supply +5V level signal or OPA +5v level for ADC input, the Conversion Register data also have 0x0000,(Config Register:0xc1e0), but when supply current 20ma for ADS1115 IN0 input and use 250 ohm between IN0 and GND(AINP = AIN0 and AINN = GND), we can read out Conversion Register data,and the result data is +5v, So I wan to know why ADS1115 have these question about it?