I'm starting a new project using the DAC8750 and need to know if the SDO pin ever enters a high-impedance state. I need to share the SPI bus with another device (EEPROM), but if the DAC8750 is always driving the SDO pin, then there will be a conflict when the other device is driving the MISO line. The DAC8750 datasheet says it is SPI compatible, but it does not indicate whether the SDO pin ever enters a high-impedance state.