Hi all,
I tried to tested the DAC161S997EVM board for getting 4-20mA current loop along with the HART modem AD5700 interface. Using the GUI softwre the DAC current is kept to be constant according to values set in DACCODE register.Then without removing the output capacitors of DAC161S997 , the HART data having UART format transmitted through HART modem (HART_OUT) is given to the C3 input capacitor of DACEVM board and from the LOOP+1 it is taken back to the ADC_IN of HART modem . But there is no HART FSK signal is coming out from the DAC161S997EVM board .What may be the reason for this???
With regards,
sruthy uk