Hi, so I'm trying to figure out a system where I'm using the ADS1294 with only two electrodes and no reference electrode and I'm a bit confused about the filtering needed (which is stressed as being important to get right). I'll be using it in full power mode where the Nyquist is said to be 256 kHz but then there is the digital decimation filter as well.
I'd prefer to do filtering in the digital domain with all things being equal too so just want to avoid aliasing without losing the signal. Is it possible to get any suggestions as I'm at a bit of a dead end? Thanks