I have a application in which i need separate voltage & current out. AVDD will be +10V to +36V, voltage output required is 0to5V & current out required is 4-20mA. No hart is required. Current loop compliance required is AVDD-2.5V. So have selected DAC8760 for this purpose.
1. IS DAC8760 right for this application.
2. Datasheet says it has only one DAC data register. So how do I right voltage & current value. Suppose I want 2V and 20mA out separability.
3. Attached is the ciruict which I had made using DAC8760 & ISO7641. Is it ok?