Hi Everyone,
I'm seeking clarity on how the ADS1299 is configured for sampling. There seems to be a "Continuous" mode which is enabled by sending the RDATAC opcode. However there is also a "continuous conversion" mode which is enabled by clearing bit 3 of register CONFIG4. Do these do different things? I can send RDATAC even if CONFIG4 bit 3 is set (enabling single shot mode).
Are these two different settings that do two different things? The data sheet is unclear. Thanks.