Hello team
From a customer who used LMP92066, the following questions came to Japan PIC.
The following URL is the datasheet of LMP92066.
www.tij.co.jp/.../getliterature.tsp
Table 12.(I2C Bus Transfer Sequence:Externally Supplied Data Sourcing Input to DACs)
is listed in page 31 of the data sheet.
Sequence_A:(Table 12.)
(1)I write the "password" in ACC_CNTL.
(2)I read the access level L2 in ACC_CNTL.
(3)I write Ox800 in DAC0*_OVRD.
(4)I write Ox400 in DAC1*_OVRD.
(5):I write 0X02 in OVRD_CTL.
The outputs are listed in the Table 12. with VDAC0=2.5V, VDAC1=1.25V.
However, really, The output are VDAC0=0V, VDAC1=0V.
Why the Sequence_A(:Table 12.) does not work definitely.
The customer confirmed the following.
Sequence_B:
(1)I write the "password" in ACC_CNTL.
(2)I read the access level L2 in ACC_CNTL.
(3):I write 0X02 in OVRD_CTL.
(4)I write Ox800 in DAC0*_OVRD.
The output is VDAC0=2.5V.
(5)I write Ox400 in DAC1*_OVRD.
The output is VDAC1=1.25V.
Please tell me the reason why Sequence_A(:Table 12.)
does not work definitely.
When the information is not enough, please contact me.
Best regards,
Keishi,Nishijima
Japan PIC