Using the ADS8556 Eval module in default HW mode and parallel xfer of Words, I am observing DB13 as a representative of the data. I have B1 set to 4VDC and the remaining 5 channels at 1VDC. I should see the 4th of 6 channel reads as a high and the others as low for this bit in the xfer. What I actually see is a high at B1's location 60% of the time, but the high is sometimes at B0 and sometimes at C0. I am not pushing the timing envelope, but I am attaching a timing diagram. Any reason that the channel alignment can bounce around?
I have all CONV tied together. STBY is tied high, RESET is tied low. AVdd=5V, BVdd=3.3V, HVdd=8V, HVss=-8V.