Hi,
I didn't find the answer to this question. Is there any internal pull-up resistor for the RESET pin in ADS129x? Can I leave it floating? I will be using the RESET command through SPI.
-Vala
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for your answer Brian. The interesting thing is that at least so far my device is working with RESET pin floating. I can read/write registers and the outputs of all VCAPs are as expected. The RESET pin also sets the registers to their default values right? For me it does not happen and the registers are read with the values that I have written (well of course that can be random). Although I don't see the DRDY signal after setting some registers and issuing the START and RDATAC commands.