This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC121C085

I´m  using the DAC 121C085  VSSOP  5V at Vref I write full-scale (FFFh) I have in the output 4.263V

If I writ (BFFh) I have 3.6V and I have 1.6V when I write (800h)

The VA pin is left float.

I'm sure the code is correct because when read back e reading value is correct.


I am forgetting something ?

Thanks for the help!

Mike