Dear Sirs,
My customer asked about DIR block of DIX4192.
Consider using contents
1. They are checking the operation as DIR which receives AES / EBU to DIX 4192 and receives 48 kHz PCM audio.
2. The DIX 4192 is used as a slave, and the master clock uses an internal PLL.
Question 1
① Can it be used as a DIR that receives 192 kHz PCM audio with the same configuration as above?
Question 2
② 48 kHz PCM audio / 192 kHz PCM audio is recognized automatically?
③ Please let me know if there are necessary setting methods with the above questions.
Best Regards,
Y.Hasebe