This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Replacing TLC2543 A toD converter with ADS7870 A to D converter

Other Parts Discussed in Thread: TLC2543, ADS7870

I am looking into two different development boards which uses TLC2543 and ADS7870 for A to D conversion. From comparing both IC's I have found out that the resolution of both is 12 bit. However, development board manufacturer mention ADS7870 being 11 bit. The data sheet of development board using ADS7870 for A to D conversion say 11 bits are used for value and 1 bit for polarity. Is that true? Is it the case with all 12 bits A to D converters ? 

  • Hi Neeraj,

    The difference is because the TLC2543 is a single ended input ADC, while the ADS7870 is a differential input ADC.  When using a single ended input the input will always be between the common pin (GND) and the Vref voltage.  Using a differential input the input (using the names of A and B for the inputs) of A will sometimes be more positive than input B and sometimes input B will be more positive than input A.  In that case the input will need to be between -Vref and +Vref.  Please compare Figure 16 in the TLC2543 datasheet and Figure 13 in the ADS7870 datasheet.

    Mike