Hello.
I would like to interface the DSK6416 with hardware that would enable wireless communication between two boards for a SIMO (Single-Input Mulitple Output) system.
To summarise what I am working on, I will have one DSK6416 as a transmitter connected to ONE antenna, and one DSK6416 as a receiver connected to TWO antennas.
This is what I have so far. The TRF3702 is a modulator that will convert the baseband signal from the DSK6416 to an RF signal. The TRF371125 is a demodulator that will convert an RF signal to I and Q baseband signals to be processed by the DSK6416. Both the TRF3702 and the TRF371125 have EVMs.
I would like to use one TRF3702 EVM for the transmit DSK6416 board and two TRF371125 EVMs for receiver DSK6416 board. The receiver board will require additional circuitry. This is because the DSK6416 has two inputs, the MIC IN (mono) and LINE IN (stereo). I require two stereo inputs because I have two TRF371125 EVMs, each representing one received signal. The two TRF371125 EVMs are connected to the one DSK6416 receive board and hence, two inputs to the receive DSK6416 boards.
I thought of using the 5-6k Interface Board for my receiver board and pair it with an ADC EVM that would take the signal from both TRF371125 EVMs and send it to the receiver DSK6416, via the 5-6k Interface board.
Is this a plausible solution to the wireless interface problem, or are there any better suggestions/solutions.
Thank you!
Best Regards.
Preia