This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Logic level shifter

Which ic is suitable for 5V to 3.3V conversion of 8-bit data.

1 Reply

  • Hello Sukumar,
    There are many devices that can do this conversion, and the best choice will depend on several factors.

    Is all the data being transmitted from 5V to 3.3V, or is some transmitting from 3.3V to 5V?

    Do any of the data channels change directions during operation? (and if so, is there an indicator line to control direction?)

    What is the maximum data rate required?

    What is the worst-case parasitic capacitance on the lines?

    How much current can the respective transmitters (3.3V and 5V) source/sink?


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.