Part Number: PGA411Q1EVM
Hi,
I am using the PGA411-EVM launchpad. All the jumpers are configured as mentioned in the user guide. I am connecting the 5V DC from the external supply using Banana Connectors. As soon as I connect those banana connectors to board the external supply is dropping around 3V to 3.3V from supplied 5V. But when I connected the EVM using USB to PC I can see the solid green light and all the fields in GUI to be correct like status connected, USB version number and PGA411 device revision numbers as mentioned in the user guide. I was also able to observe sinusoidal signals from OE1 and OE2.
But the working of the EVM is completely random. Sometimes it is working as mentioned above but sometimes I can see the solid green light and all the fields in GUI is accurate except the PGA411 device as not available, no signals from 0E1 and OE2.
The voltage drop is happening all the time irrespective of anything.
I want to know if this voltage drop is normal? If it is normal then I have some questions regarding connecting TMS320F28379D launchpad with the EVM.
If anyone has any advise, I would really appreciate it.
Thanks,
Bala.