Other Parts Discussed in Thread: REF5040, ADS8681
I have a number of question regarding the proper implementation of the ADS8691.
1) The current project contains 4 ADCs which for consistency need to share a reference. It appears that I can either create a separate RefSignal (REF5040) and bus it to each of the inputs, OR I can use the internal Reference from one of the 4 ADCs and bus it to the other 3. Is there a recommended best practice?
2) The spec Sheet for the ADS8691 includes an example layout. The layout includes a few resistor pads with connected resistors. Values are not given. How should these values be calculated?
3) On the same layout, there is an options section separated by a diode. is this section an external input, or something else. I am trying to determine if it may be useful for testing, or something else.
4) The spec sheet indicates the voltage requirements for the ADC, but i am unable to locate details on the power consumption, or current draw for either the Analog, or digital supplies. Nor how those may vary with the voltage sources. How is this to be determined?