Other Parts Discussed in Thread: ADS124S08, ADS1258, ADS131E08
I am using the ADC with the "Settling Time Using the Input Multiplexer" to read from all the channels one after the other. This has to repeat after every 8ms.
According to Figure 19 and table 14 of the ADS1256 datasheet, t_19 should last for up to a couple of hundred microseconds. But this does not necessarily mean that t_18 should also be in that range. So I would like to know what is a healthy range of t_18. For my application, as I am reading all 8 channels so I am following Figure 19 but my t_18 timing is in the range of more than 100 microseconds which is too long I guess. Is there a way to shorten the t_18 so I can reduce the overall conversion time of 8 channels?
Thanks