I have two questions about the SPI communication of the ADS1262.
1) I'm not able to sample at 38ksps, the SPI communication is too slow for that.
I'm running at 8 MHz clock which is the maximum for the ADC.
Receiving the 6 data bytes takes around 65 µs, because of that i can only sample at 15ksps max.
Any solutions for this?
2) Can I use a clock frequency higher than 8 MHz for the communication with other devices on the SPI bus?