This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DAC38J82: DAC38J82 clock input

Part Number: DAC38J82

Hello,

In the datasheet of DAC38J82 it says that the DAC clock input (DACCLK) is a LVPECT type but I have a sinewave clock generator.

Im using the LMX2531LQ2080E to generate a sine wave 2GHz, 4dBm, singel ended clock.

Can I connect the LMX2531 direcctly to the DACCLKP (and DACCLKN to 50 ohm) with the parameters above?

  • Hi Ilya,

    We are taking a look into your question, and will be back with you soon.

    Best Regards,

    Dan

  • In reply to Daniel Brock36:

    Dear Dan,
    Kind reminder...
  • In reply to Ilya Michlin:

    Hi Ilya,

    Thanks for your patience.

    Yes, the 2 GHz, 4 dBm sinewave will work as a single ended input for the DACCLK on the DAC38J82, but it is recommended that differential signals be used. With the DAC38J82EVM, I used this signal to drive DACCLKP, and tied DACCLKN to a capacitor and ground. Please note that there was not any noticeable difference when DACCLKN was left floating, but I recommend that you place a capacitor to ground.

    Best Regards,

    Dan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.