Hi:
Nowadys,I am learning how to use DAC3152EVM.and I have a question that if I connect the DAC3152EVM and TSW1400, it works properly,and I download the file "output_MultiTone.tsw" to GUI of TSW1400,clicked the button of "Send",What signal figure will I get from the DAC3152EVM of the pin"J2"or "J3"? Now I only have a digital oscilloscope ,can I use it to measure the output signal by the pin "J2" or "J3"?
There is anthoer question that in the file"DAC31X2EVM-B_SCH",there are two resistors R15 and R17 link to pin 48 (IOUTA2) of DAC3152EVM ,but they don't installed,Iwander the function of the two resistor of R15 and R17.
Thanks a lot and best wish to you!
OuyangZhao ouyang