Hello, I'm trying to configure the ADC12D800RFRB board with the wavevision dll using Matlab.
It works but only in DESI mode or NONDESI mode.
My question is exactly related with the registers 0xD43, 0xD041 and the register to configure the capture of the ADC.
for 0XD43 I use:
0xD043
0: EXT_CLK_SELECT = 0
1: DES_MODE = 0
2: CHANNEL_Q_SEL = 0
3: HW_TRIG = 0
4: IQ_CAPT = 1
for the register that I use to configure the capture (WvBoardWriteCaptureStart):
req.m_u1__ = 0
req.TransferSize = 2^12;
req.ChannelDataIndex = 2 (2 channels? for DESI is 3, may be hier is the error?)
req.HistogramEnable = 0
req.HistogramMaxBin = 100
req.DataFormat = 0
req.m_u2__ = 1
req.m_u3__ = 1
req.m_u4__ = 1
req.m_u5__ = 1
req.m_u6__ = 1
How should I capture the data with (WvBoardReadCaptureData)? should I use 2xSamples?
Thanks in advance for your help and best regards,
Gustavo